returns a list of roles in a project that satisfy the filter criteria
Get | /projects/{projectId}/roles |
Name | Description | Data Type |
---|---|---|
projectId | the id of the project to look in | string |
skip | number of records to skip for pagination | integer (int32) |
limit | maximum number of records to return | integer (int32) |
RoleID | provides a wild card string to filter roles by their RoleID. | string |
The response body is of type RolesGetResponse.
The collection of roles that satisfy the query.![]() |
RolesGetResponse
The results of the roles get query.
|
Fault | Description |
---|---|
404 | This fault returns a response body of type ProblemDetails. project with the given id is not registered on the system |